1/5/2021 2:19 AM | |
Joined: 3/3/2020 Last visit: 1/26/2024 Posts: 10 Rating:
|
Have you found a solution for this problem? We have the same issue with devices dropping in and out every 10 seconds? |
3/2/2021 1:01 PM | |
Joined: 10/23/2019 Last visit: 12/11/2024 Posts: 1 Rating:
|
Buenas también tendría el mismo error a ver si alguien lo reparo desde ya muchas gracias a todos. |
3/2/2021 3:04 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hey everybody, such errors, when IO-devices are timed out usually come when there is too much traffic on the line. there are 3 parameters that can help to lower this traffic: Send clock of the IO-controller Update time of the IO-device Watchdog-time of IO-device the terms are described here: Basic terminology of communication If the problems are on more or all IO-Devices, I would increase the Send-Clock of the IO-Controller. the update times of the devices are following this time. Update-time is a multiple of the IO-controllers send clock. When there are problems with only one devices, it may be enough to manipulate the update-time or the watchdog of this device. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to
2 thankful Users |
3/2/2021 3:07 PM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi all, there is also an FAQ for this event 02:39CB. Maybe this helps. What remedies are available if the IO controller detects sporadic, transient failures of the IO device?regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
11/19/2021 1:07 PM | |
Posts: 1 Rating:
|
Have you found the cause of this error? |
Follow us on