(0)| 5/18/2023 5:21 PM | |
|
Joined: 1/11/2023 Last visit: 9/24/2025 Posts: 7 Rating:
|
Hi Hazard_7, Sorry I need your help plase I have made an application in c# to connect to the s7-1200 siemnes plc. I connect without problem on the plc's own port. but I have added the module CP 1243-1 and in my application I have put the IP of the CP and I connect but it is very slow and even freezes the application. The plc´s own port I put 1 in slot and conecto ok and it is fast. The CP I put 1 in slot and the IP of CP is 192.168.1.135, I cant put 101 in slot. thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/22/2023 09:47:48New subject after splitting. |
|
| 5/24/2023 2:44 PM | |
|
Joined: 1/11/2023 Last visit: 9/24/2025 Posts: 7 Rating:
|
hi vic dont worry vic you need to change the number of Byte, try to put a mayor number |
Follow us on