(0)| 5/29/2009 12:05 PM | |
|
Posts: 163 Rating:
|
Hi All! The required configuration is as attached. There are two PROFINET ports(X1 P1and X1 P2)in MP377.On checking, the two ports cannot be used for redundancy. One of the port is connected to the network switch. I jus wanted a confirmation whether the other port can be used for communicating with existing Siemens Quadlog system (which runs on PCS7 HMI platform) thorugh OPC.AND HOW? AttachmentSystem configuration.zip (175 Downloads) |
Follow us on