(2)| 6/23/2023 6:50 AM | |
|
Joined: 8/3/2009 Last visit: 1/19/2026 Posts: 16644 Rating:
|
Hello Erbudak45 this sounds like a memory access violation in your scripts. Its like already mentioned, if you do not allocate enough memory for your strings or similar, then wincc writes in an unallocated memory area, this could work many times, but it is not defined where you are writing to, so if randomly a systemcritical memory area is used then the system will crash. SO this could be that it works 100 times and one time it crashes or on one system it works on other one not... If you work with C Script you should know what to do. Here are some good tipps for using strings and memory allocation: https://support.industry.siemens.com/cs/de/en/view/7929092 (And check also that any of your strings is terminated with a \n!!!) Bye Murof |
Last edited by: Murof at: 06/23/2023 06:51:35If this Information really helps, you could use the Rate function |
|
Follow us on