(0)| 6/5/2023 4:56 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, In this case I recommend creating a SR and upload the collected data via the SIMATIC Assessment Suite. See below how to collect the data. How do you efficiently collect diagnostics and system information with the SIMATIC Assessment Suite |
Last edited by: Jen_Moderator at: 06/05/2023 11:09:14Link optimized. If I could help you, you can use the RATE button. Thank you. |
|
| 6/26/2023 6:50 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi kellydekoninck, Thank you for the additional information. I do not recommend using software from other versions. If you are still running V9.0 SP2, then SFC V9.0 SP5 is not released/checked for compatibility, only SFC V9.0 SP3 Upd1 or V9.0 SP3 and you may get problems.\ I suggest you update your version to V9.0 SP3 where SFC V9.0 SP7 Upd2 can be used at most.
|
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on