(0)| 6/28/2023 2:19 AM | |
|
Joined: 5/12/2006 Last visit: 1/15/2026 Posts: 22801 Rating:
|
check the tech data https://support.industry.siemens.com/cs/ww/en/pv/6ES7517-3UP00-0AB0/td?dl=en 64 IRT Devices 512 RT Devices |
Last edited by: ChristophD at: 06/28/2023 02:20:18 |
|
| 6/28/2023 2:55 AM | |
|
Joined: 6/19/2018 Last visit: 8/12/2025 Posts: 167 Rating:
|
Is RT possible for Servo drive? and If It is possble, what is different? I mean.... for example, if RT is used, what is unusable function like synchronous control , motion control, so on? |
| 6/28/2023 5:25 AM | |
|
Joined: 1/21/2013 Last visit: 1/15/2026 Posts: 4402 Rating:
|
Hi PLC0709,
In principle, servo drives should be able to operate without IRT, but you should check with the drive manufacturer. However, using IRT will improve the quality of closed-loop position control. For example, you can find the following information in the function manual "STEP 7: S7-1500/S7-1500T Axis functions V7.0 as of STEP 7 V18": PROFINET drives can always be operated in isochronous mode or clock synchronized mode. Isochronous mode, however, increases the quality of the closed loop position control of the drive and is therefore recommended for drives such as SINAMICS S120. Kind regards |
Follow us on