(0)| 6/21/2023 8:48 AM | |
|
Joined: 8/3/2009 Last visit: 1/15/2026 Posts: 16638 Rating:
|
Hello aamirawan91 Which SD Card do you use? do you use a released Siemens SD card for HMI? Do you have formated it? Check the following FAQ: https://support.industry.siemens.com/cs/ww/en/view/95853895 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
| 6/22/2023 7:48 AM | |
|
Joined: 3/6/2022 Last visit: 7/2/2025 Posts: 119 Rating:
|
I'm not using a Siemens HMI card. Some random brand. The SD card that worked fine is not siemens either. Even the SD cards that originally came installed in the HMI with the machine were not Siemens. The Siemens manual says that you don't need to use a siemens SD card for the "data" slot. Although it's complusary to use a siemens SD card for the "System" slot. We are not using the system slot anyway. |
Last edited by: aamirawan91 at: 06/22/2023 07:48:59 |
|
Follow us on