(0)| 6/30/2022 4:45 PM | |
|
Joined: 11/23/2015 Last visit: 11/28/2025 Posts: 34 Rating:
|
Hello guys, I am facing a really annoying and strange behavior of WinCC Runtime. First of all, I am using WinCC 7.5 SP2 Upd8 on Windows 10 Enterprise LTSC 1809 OS computer. The core of my problem is that the bottom area with buttons from the standard Siemens frame is disappearing. When I start the project, I select a screen from the top area buttons, then navigate to the alarm screens from the bottom area buttons (to journal list for example) and when I decide to turn back to the work screens by selecting one from the top area buttons, the bottom area disappears(like it cannot find the .pdl). This issue is really annoying and can only be solved by turning on and off the Graphics Runtime. After that when I repeat the steps above, the result is the same. Any help and advises would be much appreciated! Best regards, Alex Attachment3.Area_Missing.zip (442 Downloads) |
Follow us on