(0)| 7/24/2023 6:46 AM | |
|
Joined: 11/7/2022 Last visit: 9/2/2025 Posts: 1 Rating:
|
Hello dchartier As you mention, "The partner PLC will be defined in Netpro along with the S7 communication connection for the S7-400H" my question is do we need to configure 4 IDs in the net pro since i did configure 4 IDs but seems only 2 of the IDs works. My configuration contain 4 setup communication, S7-400H Primary to S7-1500R Primary (ID 1), S7-400H Primary to S7-1500R Backup (ID 2), S7-400H Backup to S7-1500R Primary (ID 3) and S7-400H Backup to S7-1500R Backup (ID 4). Only ID 1 and 3 are able to set up in NetPro. ID 2 and 4 . Here attached error i got when check connection for ID 2 and 4 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/24/2023 11:29:34New subject after splitting |
|
Follow us on