(0)| 7/26/2023 6:39 AM | |
|
Joined: 12/30/2015 Last visit: 4/22/2025 Posts: 1 Rating:
|
Hi dear I have the same problem Tag logging with the script works excellent that mean when I press the button the script execute and all data on plc array write to csv file with correct format of a tag logging file... But the f(x) trend view do not show any thing and connection status is off...when change tag logging mode to cyclic trend works... Is there any special tip in trend view configuration? I Use Wincc Advanced V16.0 and S7 1212 ------------------------------------------------------------------------------------------ AttachmentHMI Problem.zip (313 Downloads) |
Last edited by: Jen_Moderator at: 07/26/2023 10:09:20New subject after splitting |
|
| 7/28/2023 12:09 PM | |
|
Joined: 8/3/2009 Last visit: 1/19/2026 Posts: 16644 Rating:
|
Hello Shta1989shta in The F(x) control you need for each value pair the exact same timestamp that WinCC will use it. Check the following FAQ: https://support.industry.siemens.com/cs/ww/en/view/109481693 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on