(0)| 7/31/2023 8:18 AM | |
|
Joined: 7/31/2023 Last visit: 9/24/2025 Posts: 5 Rating:
|
Good afternoon! When trying to establish a connection between the Siemens S7-1200 PLC and the inovance MD810 in the TIA portal, an IF configuration error occurs. The connection was configured according to the presentation in the attachment. Please tell me what could be the reason for the error? All settings are made according to the presentation, the parameters of the IF are precisely set correctly. There is an assumption that the reason for this error lies in the article number online and offline. ------------------------------------------------------------------------------------------ AttachmentScreenshots.zip (566 Downloads) |
Last edited by: Dmitry32768 at: 07/31/2023 08:25:27Last edited by: Jen_Moderator at: 08/01/2023 05:19:52New subject after splitting Last edited by: Jen_Moderator at: 08/01/2023 05:22:07All files added as .zip file. |
|
Follow us on