(1)| 8/23/2023 10:09 AM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36484 Rating:
|
S7-PCT V3.5 SP3 upd3 for IO-Link masterThe Port Configuration Tool ("PCT") is a PC-based software for parameterizing Siemens IO-Link master modules and third-party IO-Link devices. The IO-Link devices are integrated using the standardized device description "IODD" which can be obtained from the relevant device manufacturer. S7-PCT supports both IODD versions 1.0 and V1.1. http://www.siemens.com/IO-Link New functions in PCT version V3.5 SP3 update 3: The following new functions have been added compared to the previous version 3.5 SP3 Update 2:
|
This contribution was helpful to
|
|
Follow us on