(0)| 8/23/2023 7:51 AM | |
|
Joined: 10/11/2006 Last visit: 4/10/2025 Posts: 101 Rating:
|
Dear All, I have 2 S7-400 PLCs with CPU416-2 DP. These 2 PLCs are communication with each other by MPI through the X1 port of the CPU. Suddenly the communication got interrupted for about 15 to 20 seconds and came back. But this unfortunately created a breakdown in the process line due to interruption of data between the PLCs. The only thing was found is the Ethernet CP was giving fault and we reset the CP. But I believe this have nothing to do with MPI problem. I attach the diagnose report of one of the 2 PLCs. The other one is the same. Please advise what could be the reason for such problem. farra AttachmentDiagnose21-08-2023.txt (561 Downloads) |
Follow us on