(0)| 8/22/2023 7:26 AM | |
|
Posts: 14 Rating:
|
Dear All For context I am currently trying to communicate my Yokogawa AXG4A magnetic flowmeter with Siemens S7-1500 plc module via EtherNet/IP. My yokogawa sensor is EtherNet/IP based and i connected to Siemens S7-1500 via switchhub. I have set the ip of my yokogawa to 192.168.1.129 and my siemens plc is 192.168.1.100. I have search online the only workable solution is the sensor produce a unsigned 16bit value but according to electronic data sheet (EDS) the yokogawa sensor only sent out a Real Value. Therefore I am asking has anyone tried to used LCCF_enetScanner block where the siemens as act scanner and the yokogawa act as adpapter to read a real value instead of usgined int. The LCCF_enetScanner block is only accepting a unsigned 16-bit integer. When I load the program is showing no error an connected with the status of 7002, has anyone tried reading real value from EtherNet/IP sensor before and was successful at reading real value? May I know what setting or method used. My input is currently all 0. I found little information online only many are using device that produce either 16bit unsigned or boolean. Attached is the DB for LCCF_enetScanner for the adapter one the left side and output on the right side. Please find the attachement is the yokogawa sensor EDS information. sincerely Foo Brandon AttachmentAXG4A_R03007.txt (427 Downloads) |
Follow us on