(0)| 9/8/2023 11:31 AM | |
|
Posts: 359 Rating:
|
Ok ! But if I have not 1 pc. PID - regulator but 40 pcs e.g. And I want to control them from the same screen calling every PID - regulator with one of 40 buttons. What to do in this case ? Should I create 40 pcs. invisible "Picture window" one over another and somehow call them with 40 buttons e.g. Moreover WinCC assumes 32 layers only, but I need 40 "Picture windows" one over another in the same place of the screen. Is it possible to only use one "Picture window" with pdl - picture with faceplate instance inside and to control the 40 pcs. of PID - regulator ? If so, then which Script is required ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/11/2023 09:10:20New subject after splitting |
|
| 9/11/2023 9:12 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject How to control the properties of many objects in easiest way ? is published within the conference SIMATIC WinCC. Jen_Moderator |
Follow us on