(1)| 9/20/2023 11:13 AM | |
|
Posts: 13 Rating:
|
Hi Duris, I'm using TSEND and TRCV blocks to read data from a modbus server. In TRCV block, I want to give a memory area from an optimized block as DATA (InOut Variable of the TRCV block).I'm using the same structure used inside MB_Client block to send and receive data(Please find it in the attachment, and the DB in which these structures is a DB with optimized block access. I've set ADHOC TRUE and LEN to 0. But when the receive request is given I'm getting an error status of 16#8088. Please find the attachments, the program also is included for your reference. AttachmentTRCV_Attachments.zip (515 Downloads) |
Follow us on