(0)| 9/20/2023 2:27 PM | |
|
Posts: 4 Rating:
|
Hello. I am struggling on communication between Schneider VFD ATV320 and S7-1200 PLC Using Modbus TCP For starters I want to read the ETA status word from VFD, but getting 8383 error from MB_CLIENT Block I have read many topics about this error on the forum, but did not find an answer for my particular case. Im attaching a zip file with screenshots of my case AttachmentModbus TCP Problem.zip (644 Downloads) |
| 9/21/2023 6:37 AM | |
|
Posts: 4 Rating:
|
Thank you for answer. Before posting here I tried lots of combinations of LEN and Pointer. Was trying to ask 1 Len PTR 1 WORD or 2 Bytes. Was trying to PTR M1000.0 Instead of Data block. Every time the same result. Error 8383. I have found on forum that maybe changing MB_UNIT_ID to 251, or 0 or 255(default) but no luck either. I have tried changing MB_DATA_ADDR to 40001 which is empty register for that device. This is the only case when my MB_CLIENT block was getting the job DONE without ERROR Also following your tip, I have made new DB with only 1 WORD and not giving a name to it, but no luck either. Below I'm Attaching the documentation for the device I'm trying to connect with. Maybe there is something that I don't understand about. AttachmentATV320_Modbus_TCP_EtherNet_IP_Manual_NVE41313_02.pdf (664 Downloads) |
Follow us on