(0)| 9/25/2023 2:02 PM | |
|
Joined: 7/19/2022 Last visit: 1/20/2026 Posts: 436 Rating:
|
Hello AutoGen_5121707 You must enter the reference voltage in p0210. It is generally set to 380V when powered from the mains. Then it is necessary to set p0340=1, this will calculate the values of p1244 and p1248. p0340 will only be set to 0 when it has been calculated. And this should be enough. |
|
If this Information really helps, you could use the Rate function |
|
Follow us on