(0)| 9/13/2023 8:50 AM | |
|
Joined: 6/29/2017 Last visit: 10/22/2025 Posts: 7 Rating:
|
Hi! i have tried "RenameParameterSet" function, because i want to control both the name of the ParameterSet (default name when read/Create is "ParamterSet_". and ParameterSet Number/ID i first run ParameterReadAndSave and give the instruction a specific number. after i run ParameterRename to rename that same Parameterset to a specific name (to show up in the "dropdown list" in Parameter control. BUT. the rename instruction takes very long time (up to 12 seconds). do i do something wrong or can a attack my issue with something else? i have tried the rename instruction both in script and with usual function call. Thanks for answer ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/14/2023 05:42:51New subject after splitting |
|
| 9/25/2023 1:42 PM | |
|
Joined: 6/29/2017 Last visit: 10/22/2025 Posts: 7 Rating:
|
Yes i Use v18 upd 2 /Best Regards |
Follow us on