(0)| 9/27/2023 6:00 AM | |
|
Joined: 1/9/2022 Last visit: 4/24/2025 Posts: 8 Rating:
|
Hello there, i am facing the same problem. everything is working fine on local network. Please let me know if anyone found a solution for this problem. i tried the method mentioned above but still facing the same problem. i have forward the port 443 and accessing from 443 port. TIA ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/27/2023 10:13:32New subject after splitting |
|
| 9/27/2023 10:27 AM | |
|
Joined: 2/17/2020 Last visit: 1/16/2026 Posts: 1251 Rating:
|
Hi, Please check that you have the correct IIS settings set up correctly. You can see which options you need to enable here: Required Windows features for WinCC Unified You may also want to take a look at this FAQ regarding login problems. After all, even if you don't experience the specific error, you can try to do what is suggested: Error message during login in WinCC Unified Runtime You can also try closing the project in the TIA Portal and going into the project folder and deleting the folder called IM. This folder contains the compiled HMI project. And by deleting it, you force the TIA Portal to redo it all over again the next time it compiles. It is also important to have the latest Updates for your WinCC Unified (TIA Portal) version. Hope that helps! |
|
A rating will be well appreciated. |
|
| 9/28/2023 9:25 AM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello Kashif Saeed Do you have managed already a secure access? check also this FAQ: https://support.industry.siemens.com/cs/de/en/view/109810490 And check also in your certificate manager if you use the IP and Computername in the certificates because of routing or also if you use a name resolutino in the network Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on