(0)| 10/4/2023 12:21 PM | |
|
Joined: 5/5/2022 Last visit: 6/3/2025 Posts: 2 Rating:
|
Dear Experts, We have a VAT valve (attached the manual of the valve) and we want to communicate with a S7-1500 CPU. The issue is that there is no GSD file and the communication should be done through an Ethernet port. This interface enables remote operation using a command set based on RS232 commands tunneling through Ethernet.I have the complete set of the instructions that they should be transmitted. I have used on TIA Portal v16 the built in command TSEND_C. I have create a new connection and I have placed the IP of the valve on the DB that was created. I am sending a command which is of type String and it looks like p:0B0F10010000. The reason for sending such a thing is because I tried on the command line of the VAT software the command with the exact format and it worked. My questions to you are : 1) Am I correct on using the TSEND_C command? 2) The format on PLC side String is right? On the manual I didn't find something specific about this. Also I tried other types of data but they were not accepted by the compiler of TIA Portal. (pages 40- 64 for your reference on the protocol) Thank you Attachment1177507EA Manual 616 serie.pdf (497 Downloads) |
Follow us on