(0)| 10/12/2023 9:18 AM | |
|
Joined: 8/3/2009 Last visit: 1/22/2026 Posts: 16658 Rating:
|
Hello SandroAutomation 1.) I worked also a lot with tranparent buttons. The best was to use a seperat layer for all this buttons, and also they are mostly on top of other elements then a higher layer you will need any way. Then i used often the Layout functinoality of TIA Portal Screens, so you can click on the Button in the layout tree and it is selected also in the screen. But of course the dotted visualisation as in WinCC flex or Comfort/Advanced is not implemented in Unified. 2.) since TIA Portal V18 you can use events in Faceplate interfaces also. Have a look in the manual it is described how to use it, its a little bit different (work with scripts) but it works good for me. https://support.industry.siemens.com/cs/ww/en/view/109813308/160898682379 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
Follow us on