(0)| 3/10/2023 9:24 AM | |
|
Joined: 8/3/2021 Last visit: 1/23/2026 Posts: 133 Rating:
|
Simatic S7-1200 CPU, Keyence IOlink Master NQ-MP8L, 2 Slaves Keyence flowmeters FD-H32(K). - both Slaves correctly set: language, IOlink channels configuration, flow direction, etc... - NQ Sensor Monitor (Keyence utility) can find Master and both slaves, can communicate and display measured value (flow); - GSDML file of Master imported into TIA Portal; - Siemens IOlink library imported; - Keyence Master added to device configuration; - IP address of Master set; PROBLEM: - Keyence Slave needs 12 WORD INPUT data block to append to both Ports (Port1 and Port2); Keyence flowmeter FD-H32 uses 12 WORD INPUT datablock for communication; this datablock is missing in IOlink Library; it's not possible to build it from more datablocks (I can assign ONLY ONE datablock to every IOlink port); - if I try to use smaller or bigger datablock it doesn't work; - online diagnostic of CPU and IOlink Master report error; AttachmentaaaSnap.zip (651 Downloads) |
|
TIA Portal V13/14/16 |
|
| 9/19/2023 2:32 PM | |
|
Posts: 32 Rating:
|
Hi, I have the exact same problem ... Have you found the solution for this? |
Follow us on