(1)| 10/23/2023 11:13 AM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello Of course you can use filesystem to create own tsv or csv files with userdefined content. I used an own created recipe system in a past project in Unified V17 wihout using the Parameter Control system in Unified. Here I also used an Export Import function and wrote it in javascript. I used also Symbolic adressmultiplexing and with an Array of UDT which makes the Export/import quite comfortable. Examples for accessing Filesystem in Javacscript in winCC Unified are included as Snippets and also in the Tips and Tricks. https://support.industry.siemens.com/cs/ww/en/view/109758536 But of course its not an automatic function and you have to do the work by your own. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on