10/23/2023 10:43 AM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
In attachment a possible solution. Suppose you use VW100 as the address of the VM memory like I did in the attached example. Then you query the address 100 using NAI. Connect the output of the NAI to the input of an analog threshold trigger. You parameterize this so that the digital output is switched on when the value of VW100 is greater than 0 and thus starts a on delay. Once the on delay time has expired, you switch over to the analog MUX with a positive edge so that instead of the value in VW100, the value is passed on to the downstream analog network output. This will write the value in VW0 to 0. See also the attached screenvideo. AttachmentOverwrite NAI after time.zip (677 Downloads) |
Last edited by: ixo65 at: 10/23/2023 11:08:22 |
|
This contribution was helpful to
1 thankful Users |
Follow us on