(2)| 9/29/2023 1:28 PM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello fainlaip What kind of Client do you use?? You only have to insert the Client in Simatic Manager if you use a Multiclient with own project, if you use a Uniclient without an own project then you do not need to insert it, you only add the client in the Server project at Computer. Then check everything from this FAQ in all Servers/Clinets: https://support.industry.siemens.com/cs/de/en/view/868014 on the Client you just have to install WInCC and do the configuration from the FAQ and then interconnect to the Server Project. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on