11/3/2023 5:13 PM | |
Joined: 8/13/2023 Last visit: 5/13/2025 Posts: 12 Rating:
|
Hello, this is all the procedure performed by me with TIA V14 SP1, TIA V15.1 and TIA V16. In the compressed folder are all the images from the process. -From TIA Portal V14 SP1 img1_TIAV14: Information displayed from Online acces for the CPU img2_TIAV14: Creating project in TIA V14 SP1 with unspecified CPU, notice the Firmware version V4.2 as the maximum available img3_TIAV14: Hardware detected from unspecieifed CPU img4_TIAV14: Messages displayed when trying to go Online with CPU -From TIA Portal V15.1 img1_TIAV15: Information displayed from Online acces for the CPU img2_TIAV15: Creating project in TIA V15.1 with unspecified CPU, notice the Firmware version V4.3 as the maximum available img3_TIAV15: Hardware detected from unspecieifed CPU img4_TIAV15: Messages displayed when trying to go Online with CPU -From TIA Portal V16 img1_TIAV16: Information displayed from Online acces for the CPU img2_TIAV16: Creating project in TIA V16 with unspecified CPU, notice the Firmware version V4.4 as the maximum available img3_TIAV16: Hardware detected from unspecieifed CPU img4_TIAV16: Messages displayed when trying to go Online with CPU img5_TIAV16: Information shown at "Diagnostics -> Device Information" AttachmentBackup_CPU.zip (407 Downloads) |
11/3/2023 5:48 PM | |
Joined: 7/7/2010 Last visit: 9/2/2025 Posts: 16055 Rating:
|
Please review this link: |
science guy |
|
11/3/2023 6:31 PM | |
Joined: 8/13/2023 Last visit: 5/13/2025 Posts: 12 Rating:
|
Hello, this is all the procedure performed by me with TIA V14 SP1, TIA V15.1 and TIA V16. In the compressed folder are all the images from the process. -From TIA Portal V14 SP1 img1_TIAV14: Information displayed from Online acces for the CPU img2_TIAV14: Creating project in TIA V14 SP1 with unspecified CPU, notice the Firmware version V4.2 as the maximum available img3_TIAV14: Hardware detected from unspecieifed CPU img4_TIAV14: Messages displayed when trying to go Online with CPU -From TIA Portal V15.1 img1_TIAV15: Information displayed from Online acces for the CPU img2_TIAV15: Creating project in TIA V15.1 with unspecified CPU, notice the Firmware version V4.3 as the maximum available img3_TIAV15: Hardware detected from unspecieifed CPU img4_TIAV15: Messages displayed when trying to go Online with CPU -From TIA Portal V16 img1_TIAV16: Information displayed from Online acces for the CPU img2_TIAV16: Creating project in TIA V16 with unspecified CPU, notice the Firmware version V4.4 as the maximum available img3_TIAV16: Hardware detected from unspecieifed CPU img4_TIAV16: Messages displayed when trying to go Online with CPU img5_TIAV16: Information shown at "Diagnostics -> Device Information"
AttachmentBackup_CPU.zip (354 Downloads) |
Follow us on