(0)| 11/7/2023 8:07 PM | |
|
Joined: 1/21/2013 Last visit: 1/22/2026 Posts: 4427 Rating:
|
Hi JohnCass, If not already installed, please install the latest updates - currently Update 3 - for WinCC Unified V18 and WinCC Unified PC Runtime V18. If the problem persists with the installed updates, please contact Customer Support. It would be interesting - also for the support - if the error occurs in different projects or only in one project. It might also be interesting to know the status of the already loaded project in the SIMATIC Runtime Manager. If an error is reported there, this could be the reason. However, we volunteers here would need your project to further investigate your problem, so it's better to contact the support. Kind regards |
This contribution was helpful to
|
|
| 11/9/2023 2:41 PM | |
|
Joined: 8/3/2009 Last visit: 1/22/2026 Posts: 16658 Rating:
|
Hello JohnCass I also have this kind of issue if the certificates and the configuratino is not made properly on a Unified RTor Simulation system. Check this FAQ: https://support.industry.siemens.com/cs/de/en/view/109806850 Perhaps it helps Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on