(1)| 11/10/2023 10:48 AM | |
|
Joined: 4/16/2018 Last visit: 1/9/2025 Posts: 50 Rating:
|
Hello everybody, I need to upgrade a project from V15.1 to V18 but it fail directly at 1%. I already did it for another project wich was quite the same and it worded well. What I tested: - I compiled and saved the program - TIA V15 and V18 are update with the last version. When I lunch the migration all is ok and green for the service packs - I can't upgrade V15 > V16 > V17 > V18 because I don't have V16 and V17. I don't realy understand the Log file i share it with you. Some files seems to already exist ? Anybody have an idea ? CBB. AttachmentV15 to V18 error.pdf (561 Downloads) |
Follow us on