11/30/2023 8:56 AM | |
Joined: 12/23/2021 Last visit: 2/21/2024 Posts: 234 Rating:
|
Hi! Are you using WinCC Unified, right? The "Alarm control" object displays alarms that occur during the process in a plant. You can also use the alarm control to display the alarms in lists. WinCC offers various views, such as "Show active alarms" or "Show logged alarms". You can define the buttons of the alarm control in runtime and their operator authorizations in the Inspector window under "Properties > Properties > Miscellaneous > Toolbar > Elements", but some buttons are enabled by default. All the information available about this configuration is described in the manual: Alarm control |
If this post helped you in any way, please rate it positively. |
|
This contribution was helpful to
2 thankful Users |
Follow us on