(1)| 6/12/2009 8:15 AM | |
|
Posts: 10 Rating:
|
Hello Experts, Can anyone please explain me what the purpose of signal card (6DS1916-8RR) and for which application it is used for. many thanks, Naveed |
| 6/12/2009 8:48 AM | |
|
Joined: 9/27/2006 Last visit: 1/15/2026 Posts: 12481 Rating:
|
Hello Naveed: Here is the description of your part number as found on the A&D Mall: WinCC I/O signal module: OS single station and OS client can be expanded by a signal module. These signal modules can control a horn and up to 3 different lamps or buzzer tones that represent a variety of message classes. Using a hardware timer (watchdog), the signal modules can detect and signal the failure of an operator station. A hardware acknowledgment button can also be connected. The signal modules are installed in a PCI slot in the operator station.Hope this helps, Daniel Chartier |
Follow us on