(1)| 3/4/2022 4:07 PM | |
|
Posts: 1 Rating:
|
Hello sir my name is José Manuel. I have a similar problem as i am trying to install the tía portal v16 in my Windows 10 64bit sistem. So i have a folder with all the instalatión settings in my Desktop of my main Drive. I have deactivated all the antivirus and firewalls, and i have disbled the net adapter. I am starting with the instalatión of TIA portal STEP7 prof safety WinccProf v16.0 I run start.exe as administrarle and the instalatión Begines to initialice. When It reach 50%of the initialation It stop and pops Up the instalatión screen for setup where you have to select the languages of instalatión and then press Next. I press Next and then the Next screen shows. enviromentanalize MSI file initialization failed: ERROR_INSTALL_FAILURE The only options from that scren is to cancel the instalation and go back. So i have dig all internet trying to find something that helps but i havent find anything that solves the issue. I have all my files in the main Drive of muy computer. I have modified the register editor/MSI.package/Shell/runas/command/ default(msiexec /i "%1"). I have no idea which one of the MSI files its not able to install so i cant work with It. I have download the software twice just un case the First one was faulty. I need help , i beg someone like you help me. Thank you very much for your help gents its a pleasure to have you covering our backs. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/07/2022 10:16:16New subject after splitting |
|
| 10/13/2022 8:11 AM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Hi, this message often appears, if installation files (DVD or download) are "defect". Please download, or re-download the installation files again and check if installation is possible afterwards. SIMATIC STEP 7 incl. Safety and WinCC V16 TRIAL Downloadregards sancruz |
|
Feedback appreciated, please rate |
|
Follow us on