12/15/2023 5:58 PM | |
Joined: 10/13/2021 Last visit: 12/15/2023 Posts: 2 Rating:
|
Hi I have a project where i need to make some points available to the customer. So to begin I set up modbus points on 2 seperate LOGO 8.3 devices to ensure that can communicate. These were set as modbus compatible devises to simulate my real world connection I have set 1 logo to server with a client connection and the 2nd logo to client with a server connection. I then added a simple DI to network output. I cant get the 2 Logos to communicate, any help much appreciated. AttachmentModbus.zip (466 Downloads) |
12/15/2023 6:10 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
I see only one LOGO! diagram, not two. |
12/15/2023 6:56 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
In attachment a network project with two LOGO! by connection via modbus as example.
Attachment2_LOGO!s_Modbus_connection.zip (519 Downloads) |
Follow us on