(0)| 12/9/2023 10:09 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Franck; The S7-1214C can use its first 6 input as high-speed counters (HSC), with a max. frequency of 100 kHz on the first 2 HSC. The screenshot below, from the datasheet of the S7-1214C AC/DC/RLY, confirms this. This document provides details on the S7-1200 HSC: There are many posts on the forum discussing the connection of a pulse flowmeter with HSC inputs of a S7-1200. This one points to example applications that you could find useful; if you want to look at more discussions, use the search box at the right of this page. https://support.industry.siemens.com/forum/ca/en/posts/pulse-flowmeter/221002 Hope this helps, |
| 12/13/2023 10:24 PM | |
|
Joined: 2/10/2015 Last visit: 10/8/2025 Posts: 291 Rating:
|
AttachmentREAD FLOW METER PULSE.zip (406 Downloads) |
| 12/16/2023 11:40 PM | |
|
Joined: 2/10/2015 Last visit: 10/8/2025 Posts: 291 Rating:
|
Good evening Dchartier, after being inspired by the links you sent me, here is the program that I was able to write concerning the reading of the real volume of the liquid which passes through a flow meter via its pulse output with the PLC1200. Please take a look to give me some guidance on what's missing. Thank you for helping me. Sincerely AttachmentREAD FLOWMETER PULSE TO REAL VOLUME.zip (385 Downloads) |
Follow us on