(0)| 12/15/2023 1:37 AM | |
|
Joined: 10/7/2005 Last visit: 1/16/2026 Posts: 3054 Rating:
|
Physically creating a Ring without configuring MRP will indeed cause this problem. Solution is to simply follow the example as available HERE. |
|
Cheers |
|
This contribution was helpful to
|
|
| 12/19/2023 3:51 PM | |
|
Joined: 7/7/2023 Last visit: 1/15/2025 Posts: 32 Rating:
|
Everything works correctly, when I connect the ring I stop seeing all the cards, do you mean that? |
Last edited by: Jen_Moderator at: 12/20/2023 09:42:02Text formatting optimized. |
|
| 12/19/2023 7:35 PM | |
|
Joined: 7/7/2010 Last visit: 1/16/2026 Posts: 16379 Rating:
|
If everything works correctly before connecting into a ring, and you have not configured the network topology as a ring, why are you physically connecting the hardware into a ring? It is going to cause all manner of unexpected problems because there are multiple undefined paths to devices. If you want or need a ring topology, configure and enable it, then download the hardware changes.
|
|
science guy |
|
This contribution was helpful to
|
|
Follow us on