6/15/2009 6:41 AM | |
Joined: 10/21/2008 Last visit: 10/5/2024 Posts: 36 Rating: (0) |
Dear Expert, I need the operating Manual of 6RA2232-6DV62-0 DC DRIVE Thanks in Advance |
6/15/2009 7:15 AM | |
Joined: 9/27/2006 Last visit: 10/9/2024 Posts: 12285 Rating: (2685) |
Hello honey; The following link will open the Product Support webpage (see link on top of this page) in the Simoreg K 6RA22 section. These are 3 phase DC-converters, 400V, and the manuals cover more than a single model for each type. You can select "manuals" in the Entry Type to filter out the documents, and locate your required manual there. Hope this helps, Daniel Chartier |
Follow us on