(0)| 1/24/2024 11:21 AM | |
|
Joined: 1/17/2024 Last visit: 11/25/2024 Posts: 3 Rating:
|
Which one of installation logs? There is more and more errors, could anyboydy helps? I can send logs. There are installed all versions of TIA portal and few WinCC versions. from logs I already checked is not clear for me what wrong exactly. from first log ADS_SIA_Sequence_950b6.msi: MSI (c) (90:50) [12:18:52:796]: Note: 1: 2247 2: C:\windows\Installer\950b6.msi 3: 4: DEBUG: Error 2247: Database: C:\windows\Installer\950b6.msi Transform stream read/write failure. 1: 2247 2: C:\windows\Installer\950b6.msi 3: 4: This update package could not be opened. Contact the application vendor to verify that this is a valid Windows Installer update package. TrgESSPTMTOToUpgESSPTMTO MSI (c) (90:50) [12:18:52:796]: Note: 1: 1708 MSI (c) (90:50) [12:18:52:796]: Product: [MAIN_EDITIONDISPLAYNAME] - Support Base Package TO-01 V18.0 SP1 -- Installation failed. but I see this file into mentioned path. second log ADS_SIA_Sequence_SUPBASETO01.msi: MSI (c) (90:50) [12:19:28:850]: Note: 1: 2247 2: G:\InstData\SUPBASETO01\Media\SUPBASETO01.msi 3: 4: DEBUG: Error 2247: Database: G:\InstData\SUPBASETO01\Media\SUPBASETO01.msi Transform stream read/write failure. 1: 2247 2: G:\InstData\SUPBASETO01\Media\SUPBASETO01.msi 3: 4: This update package could not be opened. Contact the application vendor to verify that this is a valid Windows Installer update package. TrgESSPTMTOToUpgESSPTMTO MSI (c) (90:50) [12:19:28:850]: Note: 1: 1708 MSI (c) (90:50) [12:19:28:850]: Product: [MAIN_EDITIONDISPLAYNAME] - Support Base Package TO-01 V18.0 SP1 -- Installation failed. but I see this file into mentioned path. Third log SIA_Starter.log and fourth one SIA_STEP7_S7FPLUS_WINCC_ADV_V18@24-01-24_12-17-07.log attached. There is more errors. ------------------------------------------------------------------------------------------ AttachmentSIA_Starter.txt (271 Downloads) |
Last edited by: aginko at: 01/24/2024 11:38:48Last edited by: Jen_Moderator at: 01/26/2024 10:06:14New subject after splitting |
|
| 1/24/2024 11:23 AM | |
|
Joined: 5/12/2006 Last visit: 1/31/2026 Posts: 22836 Rating:
|
the latest one in the directory %AUTINSTLOG% |
| 1/24/2024 11:39 AM | |
|
Joined: 1/17/2024 Last visit: 11/25/2024 Posts: 3 Rating:
|
fourth one SIA_STEP7_S7FPLUS_WINCC_ADV_V18@24-01-24_12-17-07.log
AttachmentSIA_STEP7_S7FPLUS_WINCC_ADV_V18@24-01-24_12-17-07.txt (288 Downloads) |
| 1/24/2024 11:42 AM | |
|
Joined: 5/12/2006 Last visit: 1/31/2026 Posts: 22836 Rating:
|
maybe corrupt instaallimage download it again and try it |
| 1/24/2024 12:05 PM | |
|
Joined: 1/17/2024 Last visit: 11/25/2024 Posts: 3 Rating:
|
same error. on downloaded ISO, and tested also installation from two original DVD. |
Follow us on