(2)| 1/31/2024 7:43 AM | |
|
Joined: 1/21/2013 Last visit: 1/16/2026 Posts: 4405 Rating:
|
Hi Jasner, In general, the scaling of analog values has not changed between classic STEP 7 and STEP 7 in TIA Portal. There are some analog modules that allow you to change the scaling in the hardware configuration, but the default setting is always "S7 style". You can still use SCALE/UNSCALE instructions, but if you are using an S7-1200/1500, it is recommended to use NORM_X/SCALE_X (see FAQ). Or you can use a more flexible version available from the support site. Kind regards |
This contribution was helpful to
|
|
Follow us on