(0)| 3/15/2022 1:02 PM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Dear Roby, new cpu's do not have a ip-address. You can open TIA -> project view -> Online access -> specify used interface -> and search for accessible devices with "Update accessible devices". Afterwards you can connect to the cpu and set up an ip-address. Or you can use a seperate tool like SINEC PNI Basic to initialize the ip-address of the cpu the first time. Or create a new project, add the cpu and download the hardwareconfig the first time. Afterwards the cpu has the ip-address configured in hw-config. SINEC PNI Basic V1.0 Service Pack 1 Update 1 Software Downloadregards sancruz |
|
Feedback appreciated, please rate |
|
Follow us on