(0)| 1/26/2024 6:30 AM | |
|
Posts: 6 Rating:
|
Hello Everyone, I am facing same issue but bit different. I have two identical systems with PLC CPU1215C and HMI TP1200. System 1 is healthy and System 2 HMI was factory reset done without taking backup. So, I have taken backup of System 1 HMI (which is healthy) and restore to System 2 (which was factory reset). After power ON of System 2 HMI it is showing ###. So, whether I have to load PLC backup also from System 1 to System 2. Note: We don't project backup, I have taken upload from PLC and HMI. Also, PLC is write protected ( So, I will have to factory reset PLC also) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/26/2024 12:31:37New subject after splitting |
|
Follow us on