11/30/2020 7:00 PM | |
Joined: 9/23/2005 Last visit: 9/24/2025 Posts: 4416 Rating:
|
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Frequently in the automation process it is necessary to set a set-point our read the actual value of a PLC's timer. The WinCC unified supports the PLC's time format and automatically adapt the IO field to show and input time values in theirs different units (ms, seconds, minutes, hours or even days). TIP: When the unit is not explicitly expressed online, the value is understood as second unit. This simple sample bring a S7-1500 with a timer (TON), whose values are represented on the WinCC Unified. Here there are also a internal time variable and buttons with scripts to decompose it in their basic sub types (ms, seconds, minutes, hours, days) and vice versa. Project (archived and ziped). AttachmentTimers.zip (1382 Downloads) |
Last edited by: Denilson Pegaia at: 11/30/2020 19:16:55Denilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
2/2/2024 1:37 PM | |
Posts: 3 Rating:
|
what about tof and tp, its not working |
Follow us on