(0)| 12/1/2008 2:30 PM | |
|
Posts: 993 Rating:
|
Hi Carmamezo, do you get any errors while publishing your pictures? Cumu |
| 12/12/2008 4:51 PM | |
|
Posts: 1275 Rating:
|
Hi CBo, I had searched for the possibility to see the web user's name in v6.2, 'cause I too thought it was only available from v7 on, but I found out in the release notes that it was already available in v6.2... Check out this session: 1.3.5 Computer-local Tags At the properties of internal tags, their updating can be set as computer-local or project-wide. With the Web Navigator V6.2, these settings are also utilized on the Web client, resulting in each client possessing its own computer-local tags. It becomes thereby possible, for example, to determine the user currently logged onto the Web client.But I haven't used this version of WebNavigator to test this... does it work? Best regards, Danielle |
Follow us on