4/8/2024 6:39 AM | |
Joined: 3/14/2008 Last visit: 9/19/2025 Posts: 2217 Rating:
|
Hi, First, you need to register the SID. This is a unique system identifier which makes it easy for siemens to provide support (one of the perks). Second, you need to put in the SID in the multiproject settings (right click Multiproject->Properties. There is a column to enter the SID. Please note: Up to PCS7 V9.x, the SID is not mandatory and the only thing you get is an annoying popup, but as of PCS7 V10, the SID is mandatory in order to run a project. |
Last edited by: Oreca at: 04/08/2024 06:41:09If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
Follow us on