4/16/2024 12:57 PM | |
Joined: 6/29/2018 Last visit: 8/28/2025 Posts: 23 Rating:
|
[snip] By the way: I would rather like to output the sign of r2521[0] to a digital output. I have a modulo axis and would like to read in externally the zero crossings of position signal. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/17/2024 08:04:46New subject after splitting Last edited by: Jen_Moderator at: 04/18/2024 05:50:46Division of questions into separate topics. Headline optimized. |
|
4/17/2024 7:31 AM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello, please check, if a TM41 would be suitable for your application. You can find a function description in the SINAMICS S120 Function Manual for Drive Functions in chapters 8.25.2 to 8.25.4. |
With best regards, |
|
4/17/2024 3:57 PM | |
Joined: 6/29/2018 Last visit: 8/28/2025 Posts: 23 Rating:
|
Actually, I programmed the task with TM41 already. See appended PDF. BUT: The sampling times internally are set by default to 4ms. => the idea to output the phase of the axis position to a HW port and try to sync with another device is not possible! Please correct if I am wrong. AttachmentProvide_position_sign_signal.docx.pdf (513 Downloads) |
Last edited by: Papa123 at: 04/17/2024 16:02:11Last edited by: Jen_Moderator at: 04/18/2024 05:55:00Division of questions into separate topics. Last edited by: Papa123 at: 04/24/2024 15:35:19 |
|
Follow us on