4/23/2024 2:15 PM | |
Joined: 1/20/2024 Last visit: 4/22/2025 Posts: 8 Rating:
|
Everytime I try to open this same project in simatic manager 5.7(running on win10), the software show those messages, and I cannot make any modifications software or hardware. When I open it in older versions like 5.5, no messages are shown and everything is ok, I can make modifications. I already tried in different VMs. The VM where the 5.5 is installed don't even have Project Messages.
AttachmentPictures.zip (426 Downloads) |
4/24/2024 4:44 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, most likely, you will need S7-Project Messages. You can also try the workarounds from this FAQ. When you open a project in STEP 7 V5.7, why do you get the error message 3280:709 "Project or library are on a write-protected medium or are protected by a rights assignment"?regards sancruz |
Feedback appreciated, please rate |
|
Follow us on