(0)| 4/25/2024 2:19 PM | |
|
Joined: 5/6/2022 Last visit: 1/15/2026 Posts: 589 Rating:
|
Hi Landon1220, In this case, I would recommend that you review the following FAQ that I share below since it explains in detail the options that exist to perform an upload: On the other hand, in principle when you connect online with the PLC it usually tells you the version with which the project was loaded. Best regards! |
|
If this Information really helps, you could use the Rate function |
|
| 4/25/2024 2:21 PM | |
|
Joined: 9/21/2012 Last visit: 1/19/2026 Posts: 4855 Rating:
|
You need to upload the project with TIA15.1. You can't open a TIA18 project file with older TIA versions. |
Follow us on