(0)| 1/24/2022 12:08 PM | |
|
Posts: 2 Rating:
|
Well i have the same problem : I want to install the Sinema RC server on cloud (AWS). But I need to install the version 2.0 (because I want to connect a cp 1243-7 LTE device). But from the version 1.3, there is a dualboot then I can't install the server on AWS. Then do you know if it's possible ? If I can install the server on AWS ? Is that not possible even if I buy a licence ? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/24/2022 14:21:01New subject after splitting |
|
| 1/24/2022 3:49 PM | |
|
Joined: 4/25/2017 Last visit: 1/21/2026 Posts: 445 Rating:
|
Hi, SINEMA RC Server in the cloud is only possible from V3.0 or higher. Here is a manual how to do it: |
|
Best Regards, |
|
| 1/28/2022 9:55 AM | |
|
Joined: 8/3/2009 Last visit: 1/22/2026 Posts: 16661 Rating:
|
Hello here are also a few information, but I think unfortunately also only since V3.0 https://support.industry.siemens.com/cs/de/en/view/109801210 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
| 4/26/2024 6:16 AM | |
|
Joined: 4/2/2021 Last visit: 12/19/2025 Posts: 4 Rating:
|
Anyone Success install |
Follow us on