(2)| 11/21/2025 9:40 AM | |
|
Joined: 8/14/2020 Last visit: 1/14/2026 Posts: 451 Rating:
|
Hello,
Can the PLC be pinged from the IPC? If so, check the PG/PC interface in the Control Panel. It should be set to S7online and the network card (TCP/IP) connected to the PLC. https://support.industry.siemens.com/cs/us/en/view/11870489 If you can't get this to work, please send screenshots of the PG/PC interface. System messages in WinCC Advanced are also helpful; please send screenshots of those as well. Best regards, Costanza |
Follow us on