(0)| 6/24/2009 4:15 AM | |
|
Posts: 160 Rating:
|
The only limitation is that the external DP master supports routing and as you can see in the attached link for the technical details it does. http://support.automation.siemens.com/WW/view/en/29713139/td Therefore accessing the S120 will be possible. Of course you will need to integrate the S120 into the project with the IM151-8F to be able to do this with Drive-ES Basic |
| 6/24/2009 7:36 AM | |
|
Joined: 3/21/2006 Last visit: 1/23/2026 Posts: 10248 Rating:
|
Hello Berg, Perhaps following FAQs are helpful: Routing with DriveES Basic (STARTER or DriveMonitor) in a STEP 7 multiproject. How is a routing established from one PG via a PROFIBUS interface through a SIMATIC station to SINAMICS G120/G120D frequency inverter via a PROFINET interface? Regards Hristo Mihalev |
Follow us on