7/8/2024 12:02 PM | |
Joined: 8/3/2009 Last visit: 9/10/2025 Posts: 16386 Rating:
|
Hello H.SAPER The dashed thick green lines are ethernet communication connections like HMI connection or PLC connections. It is always shown if you select one communication connection or IO Communication between the partners. Here are a few information: https://support.industry.siemens.com/cs/ww/en/view/109815056/161014765195 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on